cancel
Showing results for 
Search instead for 
Did you mean: 

Debugger starts up at wrong address.. sometimes..

texton1
Associate II
Posted on March 22, 2016 at 17:39

Hi All, 

I just started working on a STM32L151. I've setup the debugger to break at first instruction (not main), but when I start debugging the program counter stops at 0x1ff00b84 which isn't even a part of the flash (starting at 0x8000000). 

It gets wierd, because when i try resetting the debugging session (without downloading the program again), a couple of times it finally stops at the first instruction in my startup-file (startup_stm32l1xx_md.s) and everything runs smoothly until the next time I need the program the device and start the debugger again. 

I am really at the bare bottom here, and it really begins to take up time on the project. 

I use CoIDE with the compiler ''GNU Tools ARM Embedded 4.8 2014q2''. 

And I run on some custom HW that just arrived - though I've worked with STM32F for a some time, and never seen anything like it.. 

I've attached the startup file I'm using, if that helps.. 

Hope someone has an idea?

#stm32l151
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on March 22, 2016 at 17:53

Hope someone has an idea?

State of BOOT0 pin at reset?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
texton1
Associate II
Posted on March 22, 2016 at 18:40

Oh, of course! It was flying (HW mistake), and I've just tried to pull it to ground - everything is working just fine.. 

Thank you very much! :) :) :)