STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem with USB migrating from stm32f072 to stm32f042

Posted on November 02, 2016 at 22:18I have a USB CDC project that works fine with the STM32F072-DISCO board, but when I try to migrate the code over to my own board with an STM32F042 on it the device shows up as an ''STM Device in DFU Mode'' instead...

hampton by Associate II
  • 1197 Views
  • 2 replies
  • 0 kudos

__HAL_LOCK routines with no __HAL_UNLOCK

Posted on November 03, 2016 at 15:39Hi,__HAL_LOCK has never bothered us previously with v 1.3 HAL library.However, I have updated to 1.5.1 STM32F7 lib and found that stm32f7xx_hal_sai caused us problems.It was related to the handle being kept locked...

AndyJT by Associate III
  • 1111 Views
  • 1 replies
  • 0 kudos

STM32F030 UART TX via DMA only works once

Posted on October 31, 2016 at 22:25 Hi, I've seen similar questions to this but none seem to have helped. I'm transmitting on UART1 via DMA channel 2 and the first transmission works fine. I am unable to get anything out after receiv...

STM32F0 ADC Timer Triggered conversion hangs

Posted on November 03, 2016 at 15:41 Hello I am trying to use TIM3 update event to trigger ADC to convert one channel 1000 times @ 50kHz resulting in about 20ms. This is for filtering out net interference. The problem is when I configu...

rwa by Associate
  • 1281 Views
  • 2 replies
  • 0 kudos

Resolved! STM32Cube doesn't copy 'Drivers' files in project

Posted on October 28, 2016 at 09:13Hi. I've generated a project using Cube, but the Drivers directory is void (it has subdirectories but any file), and then the project is full of errors. I've attached the project. The project properties are: - STM3...

jmasriera by Associate II
  • 2249 Views
  • 2 replies
  • 0 kudos

Problem BOOT

Posted on November 03, 2016 at 14:25Hi all! I have a problem with STM32 BOOT (I used a STM32F207). If the microcontroller restarts (after power-off), the firmware is blocked during the CLK initialization (and RTC initialization). I changed capacito...