cancel
Showing results for 
Search instead for 
Did you mean: 

Reading ADC lower amplitude values

hitsumen
Associate II
Posted on May 31, 2016 at 13:38

Good day,

I am trying to read sinus from audio line in.

But I see that I could only read higher value of my amplitude, here is the example:

http://s33.postimg.org/i5ew1ozgf/sin.jpg

My source code:

#define IO_PIN       GPIO_Pin_5

#define IO_PORT      GPIOC

#define IO_PORT_CLK  RCC_AHB1Periph_GPIOC

#define ADC_CLK      RCC_APB2Periph_ADC1

#define ADC_NUM      ADC1

#define ADC_CHANNEL  ADC_Channel_15

void ADC_start_test(void)

{

   ADC_SoftwareStartConv(ADC_NUM);

}

void ADC_init_test(void)

{

 

GPIO_InitTypeDef GPIO_InitStructure;

 

ADC_CommonInitTypeDef ADC_CommonInitStructure;

 

ADC_InitTypeDef ADC_InitStructure;

   /* Enable peripheral clocks */

   RCC_AHB1PeriphClockCmd(IO_PORT_CLK, ENABLE);

   RCC_APB2PeriphClockCmd(ADC_CLK, ENABLE);

 

   /* Configure ADC Channel 10 pin as analog input */

   

   GPIO_InitStructure.GPIO_Pin = IO_PIN;

   GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

   GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

   GPIO_Init(GPIOC, &GPIO_InitStructure);

 

   /* ADC Common configuration *************************************************/

   

   ADC_CommonInitStructure.ADC_Mode = ADC_DualMode_RegSimult_InjecSimult;

   // APB2 clock is half the 168Mhz system clock (i.e. 84Mhz),

   // so with a div by 8, ADC PCLK would be 10.5Mhz.

   // F4 datasheet says ADC clock freq should be 0.6Mhz - 30Mhz for Vdda=3.3V

   ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div8;

   ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

   //TwoSamplingDelay is only used in dual and triple modes)

   ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;   

   ADC_CommonInit(&ADC_CommonInitStructure);

 

   /* ADC1 regular channel 10 to 15 configuration ************************************/

   

   ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

   ADC_InitStructure.ADC_ScanConvMode = DISABLE; // 1 Channel

   ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; // Conversions Triggered

   ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; // Manual

   ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T2_TRGO;  //Unused for manual?

   ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

   ADC_InitStructure.ADC_NbrOfConversion = 1;

   ADC_Init(ADC1, &ADC_InitStructure);

   //The sample time is how long the input is sampled before the conversion is done.

   //Since PCLK is 10.5Mhz, 144 cycles is about 13.7uS and the DAC output rate is

   //running manually off a 44Khz timer interrupt (22uS), we should be fine

   //(once conversion starts, it takes about 16 cycles)

   ADC_RegularChannelConfig(ADC_NUM, ADC_CHANNEL, 1, ADC_SampleTime_144Cycles);

 

   /* Enable ADC1 */

   ADC_Cmd(ADC_NUM, ENABLE);

   ADC_start_test();

}

//Get ADC value if the ADC is ready

//Returns value if successful, -1 if ADC wasn't done yet

uint16_t ADC_get_test(void)

{

   //HACK - TESTING

   while (ADC_GetSoftwareStartConvStatus(ADC_NUM) != RESET)

      ;

   //HACK - TESTING

   

   return (ADC_GetSoftwareStartConvStatus(ADC_NUM) == RESET)

      ? ADC_GetConversionValue(ADC_NUM)

      : -1;

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 31, 2016 at 14:41

What am I looking at?

The ADC isn't going to work with negative voltages, and likely violates the specs.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..