STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem sending online support request

Posted on November 12, 2016 at 18:26HelloThere seems to be a problem sending online support request, when i try to log in to request page i face this message:We're sorry, but the last operation caused an error.You did not have a privilege required t...

How RESET address is determined in STM32?

Posted on November 10, 2016 at 05:25Hi, I know that when a stm32 mcu resets, it first jumps to address 0x0 where a vector table resides. And then it jumps to reset handler. My question is, how is the vector table flashed at address 0x0 ? Is it decid...

Current consumption and state of GPIO in StandBy mode?

Posted on November 11, 2016 at 18:35For the STM32F0 device, in the standby mode after executing the function HAL_PWR_EnterSTANDBYMode(), will all the GPIO pins (except for the wakup pin and RTC tamper ...) are put in highZ mode?  Or is it something ...

Vu.Andy by Associate III
  • 797 Views
  • 0 replies
  • 0 kudos

The example of receiving ethrnet frames

Posted on November 08, 2016 at 09:43Hi!I am the beginner in ethernet on STM32F407.I connected STM32F407 to LAN8720, LAN8720 connected through ethernet cable to PC.   I set IP-address 192.168.0.10 (255.255.255.0) for the PC and on the PC I did ping 1...

Stop Mode and Spi Peripheral Behaviour

Posted on November 11, 2016 at 11:50Hello Everyone,In our application , Radio is connected to  stm32f4 series MCU via SPI and radio Irq line connected to one of the Exti line of mcu. Before putting into the stop mode, radio has been configured . Upo...

STM32F746 Discovery transfer data via Ethernet

Posted on November 10, 2016 at 19:39Greetings!We are having a project in our class where we are using a  STM32F746 touch system. We have programmed a code where we store some data on a file. I am wondering if anyone could guide me to how to transfer...