cancel
Showing results for 
Search instead for 
Did you mean: 

[Resolved] HAL_IncTick() Preempt Priority problem when use other timer as timebase

diverger
Senior
Posted on June 17, 2016 at 04:54

I've noticed from STM32CubeMX V4.15.1, when I choose other timers except system tick timer as timebase source. The macro 'TICK_INT_PRIORITY' is defined as 0 (highest). And I can't figure out how to change it. But when use systick timer, the priority can be changed in the NVIC wizard. 

Before 4.15.1, it's default to 15.

Why??

#timebase #systick
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Walid FTITI_O
Senior II
Posted on June 17, 2016 at 14:21

Hi diverger,

I have made a quick test on the STM32CubeMx 4.15.1 , I select a timer as time base source, I open the NVIC Configuration and everything goes fine ; By default, subpriority is 0  I can select the pre-emption priority from 0 to 7. To modify the sub priority form 0 to 1/2/3/4 , you should change the ''priority group'' on the top and select one of the 5 alternatives depending of the number of subpriotity and pre-emption priority that you would select.

-Hannibal-