STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA and RCC Low Power Enable bits (LPENR)

Posted on November 17, 2016 at 20:02I'm on an STM32F4 and using an RTOS.  I put the MCU to sleep whenever the scheduler has nothing to do using the WFI instruction.  I'm using DMA1 with i2S and a USART.  I want to disable the DMA1 clock using the RC...

Possible bug in Cube Lib 1.6 with I2C / DMA

Posted on November 17, 2016 at 18:22 Hello In stm32L1 Cube lib 1.6. In the interrupt handling of a transfer complete on i2c in slave mode with DMA, the HAL_DMA_IRQHandler(...) calls XferCpltCallback(...) which points to I...

JulienD by Senior
  • 733 Views
  • 0 replies
  • 0 kudos

STM32F0 UART MODBUS mode fix

Posted on November 16, 2016 at 19:42 Hello there, I was trying to get going with ModBus RTU communication on the STM32F030 chip, specifically the t3,5 interval counting, since its supported by hardware in this chip (RM0091 page 701 on the bo...

I2C module hangs on STM32F030K6

Posted on November 02, 2016 at 09:25Hello all.I've got a problem using I2C1 module on STM32F030K6 MCU. Everything works properly until I enter ESD exposure to the pcb. This leads to I2C hanging, but other parts of MCU continue working.I tried to res...

ap1011 by Associate
  • 906 Views
  • 1 replies
  • 0 kudos

Which API use for RTOS?

Posted on November 17, 2016 at 12:57Hello, The STM32cubeMX code generator labels as FreeRTOS the RTOS functionalities, but the code generated looks compliant to the CMSIS-RTOS API. The directory Middlewares\Third_Party\FreeRTOS\Source contains the s...

HELP_STM32F4DIS and HC SR04

Posted on November 17, 2016 at 14:26 I comunicate stm32f4dis with hc sr04 but always distance_mm=0, PB1-Trig PB0-Echo #include ''stm32f4xx.h'' GPIO_InitTypeDef GPIO_InitStructure; void GPIO_Configuration( void ); void ...

kakaducsy by Associate II
  • 1211 Views
  • 0 replies
  • 0 kudos

STM32F103 xl option bytes

Posted on November 17, 2016 at 13:39I'm unable to program the option bytes from user software. In an STM32F103RGT7.Erase works, program does not.Code:// Lock and unlockFLASH->CR = FLASH_CR_LOCK;if( FLASH->CR & FLASH_CR_LOCK ){  // Unlock fpec       ...

Jeroen3 by Senior
  • 933 Views
  • 0 replies
  • 0 kudos

STemWin

Posted on September 07, 2016 at 23:27Hi, I wonder if there is any chance for stemwin 5.30 or newer in near future ?Thanks

How to configure GPIO input?

Posted on November 14, 2016 at 21:35Good day,What I want is: If I put GND to GPIOD_4 I want to LED ON.If high impedance then LED OFF.I attached my schematic with CHRG pin connected to GPIOD_4.Is it possible to pull up internally gpio?I wrote some co...

hitsumen by Associate II
  • 2086 Views
  • 2 replies
  • 0 kudos