STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO L152RE Hardware version

Posted on October 27, 2016 at 14:06Hi!I have three Nucleo-L152RE Board with this features:- Board 1 and Board 2:  STM32L152RET6GH23W, Hardware version: MB1136 C-02- Board 3: STM32L152RET6GH245, Hardware version: MB1136 C-03I made a program that use ...

Microcontroller programming issue after connecting VBUS

Posted on November 04, 2016 at 14:19HeyI am using STM32F429VIT6. I have ported the USB_CDC program from the example and was working fine with the Evaluation board. I have changed the program to work with the MCU and ported the program. I havent enab...

dixon by Associate II
  • 1201 Views
  • 1 replies
  • 0 kudos

STM32F7 HS-USB ULPI PHY options from Microchip

Posted on November 12, 2016 at 20:34Hello, you may remember STM32F2 and F4 had troubles with some HS-USB ULPI transceivers from Microchip. I wonder if these issues exist with STM32F7 too ? I'm especially interested in USB3317 and USB3343. I've notic...

STM32F427 FMC connected SDRAM

Posted on November 17, 2016 at 12:16Hi guys, we have a IS42/45S16100H device connected to STM32 FMC bus ( BANK2 ). If we run the application from internal SRAM everything is fine. Unfortunately, if we use the SDRAM as heap, we have trouble. Someti...

ADC reading value

Posted on November 17, 2016 at 18:26Why if i put a voltage equal to 1V to the ADC input of the microcontroller, i read a value equal to 1.4 V??It seems that the Voltage_Actual_Value=0.7*ADC_ValueThanks #more-facts #!stm32-!adc #please.

STM32CubeMX Clock configuration error

Posted on November 14, 2016 at 16:59Hi guys,I want to use the internal 8MHz HSI reference for generating my clocks, but allthough there is now clock speed error to resolve I still get an error that the HSI is not recommended for the PLL as input. Wh...

STM32F429 external SDRAM issue

Posted on November 14, 2016 at 10:38Hi All,I have a custom hardware dev board which includes an SDRAM (AS4C16M16SA), NOR Flash (S29GL128S) and a STM32F429. The schematic for this board is identical to other commercial dev boards that have the same m...

Can i interchange two chips in same serie?

Posted on November 16, 2016 at 01:19I am using STM32F411RET6 and RCT6 chips. For some reasons, I can't tell the chip number in the board because it is blocked by something else.Therefore I present all the chips are RCT6, which has a smaller code spa...

rwmao by Senior
  • 1939 Views
  • 3 replies
  • 0 kudos

STM32F407 Infrared receiver

Posted on November 16, 2016 at 21:14I am looking to implement receivers for infrared remote control protocolsusing STM32F407 bord.However all my attempts failed.  Anyone can help my write a simple code to read the sensor input ?? Appreciated , thank...

ilyesfraj by Associate II
  • 1620 Views
  • 3 replies
  • 0 kudos