cancel
Showing results for 
Search instead for 
Did you mean: 

Internal Clocking and Sample Rate on STM32F4 ADC

epalaima
Associate II
Posted on July 01, 2016 at 18:59

Hi, I was wondering how the built in ADC on the STM32F4 was clocked, and how I could go about checking it's clock frequency.

I know that the sample rate is configured by dividing the clock (e.g.

ADC_SampleTime_480Cycles).

So I'd like to figure out the clock rate and thereby be able to set a specific sample rate.

#clock #adc #sampling-rate
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on July 01, 2016 at 20:45

Ok, so that time plus the 12 cycles for a 12-bit conversion. The clock going to the ADC is from the APB/AHB to which it is attached, that is divided down by the prescaler you can chosen for the ADC. So cycles of the clock coming out of the scaler/divider. So if that is 14 MHz, then 492 cycles of that.

If you want samples to occur at a specific clock or sample rate, you'd want to setup a timer and use that to trigger the start of the conversion. The converted value can then be services by an EOC interrupt, or by a DMA transfer to a memory array. If sample more than one channel you will need to use DMA

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..