User Activity

I updated from version 1.8.0 (compilation was ok) to version 1.9.0 where I get 2017 errors :-o.Apparently and issue with ld.exe..tools\arm-none-eabi\bin\ld.exe: SV-F777.elf section `.bss' will not fit in region `SRAM' Processor STM32F777VITxDo you ha...
Hello,CPU: ST STM32L151VCI do the following process:Starting from a running program I jump into DFU modethen STM32_Programmer_CLI -c port=USB1 -d "newprogram"then STM32_Programmer_CLI -c port=USB1 -s program start, but if I check the two first byte o...
Hello I'm migrating my STM32F072 project to the STM32L072.In my original project (F072) I can jump to the DFU bootloader by software via a function located before SystemInit.I tried to convert this to be used by L072 by changing the address of bootlo...
I have two configuration, one for debug and one for release,Debug is the first one, when I change to release IDE doesn't care about that and continue to use Debug compilation parameters.It's really boring and dangerousCan you check on your side?Thank...
When STM32CubeIDE started it propose me to select between STM32F072C8Tx or STM32F072C8Ux ...only these choice nothing more. I took the first one, telling to myself that I can change that after.But I cannot the MCU setting is greyed and fix to STM32F0...
Kudos from