cancel
Showing results for 
Search instead for 
Did you mean: 

Tj for suffix 6 & 7 in stm32 family

frankyang9
Associate
Posted on July 22, 2016 at 03:12

Hi All,

The Tj range for suffix 6 is -40~105 & suffix 7 is -40~125, is this true for all stm32 mcu family?

Thanks
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on July 22, 2016 at 10:29

Hi Frank, 

I think that it is the same, but you have to refer always to your related datasheet to confirm it.

Could you please tell us why do you need such general information?

-Syrine-