STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timeout error trying to connect via ''external mode''

Posted on April 01, 2015 at 18:22Hi, I posted a question yesterday which was solved by myself about the external mode connection. But now I am getting another problem, a timeout error. I am using the ''Embedded Coder Support Package for STMicroelect...

Trouble Resetting Nucleo-F091

Posted on December 10, 2016 at 00:53Hi Everyone.I have a very strange problem with a Nucleo-F091RC board. I've been playing around with a serialprogram just to print messages via the uart, just to get the first project started. I noticed as long as ...

kvresto by Senior
  • 1881 Views
  • 9 replies
  • 0 kudos

Image to byte converter of STM

Posted on December 13, 2016 at 17:00Hi,I am interested with web server raw.I need converter image to byte array of ST.Where can I find that program?thanks.

ali2399 by Associate II
  • 1765 Views
  • 2 replies
  • 0 kudos

UM1734 - Issue with the ''Usage'' description?

Posted on December 13, 2016 at 21:59Is it just me or is the ''Usage'' stuff mostly upside down and backwards? Me - I'm tending to believe the README.  ------------------------------------------------UserTxBufferManual UM1734:README.TXT:- 1 x Bulk IN...

0690X00000605q6QAA.png 0690X00000605q2QAA.png

STM32F4-Discovery EEPROM emulation demo does not work

Posted on December 07, 2016 at 03:21I have STM32F4-Discovery board. (MB997B with Discovery-MO expansion board)From STM32Cube package, I ran several examples, applications and demo successfully. But EEPROM_Emulation application does not work well.STM...

hansuk by Associate
  • 1965 Views
  • 3 replies
  • 0 kudos

LQFP144 pinout overlap

Posted on December 10, 2016 at 20:57So it happens that i have an overlaping pins if I try to connect an sdram 16Mx16bit an an 24bid RGB LCD. Will there be any major complication if I connect overlaping LCD bit to ground? Do i have to cange software ...

luchiann by Associate
  • 1045 Views
  • 2 replies
  • 0 kudos

STM32F030K6T6 support touch library?

Posted on December 12, 2016 at 12:00hiin this doc en.DM00210526.pdf there is no name of STM32F030K6T6 to know which pin is which Chanel of touch.and in STM32F030K6T6.pdf there is no name of touch in pin configuration.can i use touch library on this ...

How to Turn off all clock of STM32L0xx ?

Posted on December 12, 2016 at 14:43Hello,I am using STM32L0xx MCU in stop mode. but can able to achieve low power as given in datasheet?Please help me to turn off clock and also i want suggestion to achieve it.Thank you in advance. #turn-off-all-cl...