Skip to main content
piotr239955_st
Associate II
June 20, 2016
Question

STM32 shutting down debug session when CMSIS and USART works together

  • June 20, 2016
  • 1 reply
  • 545 views
Posted on June 20, 2016 at 23:16

Hi

I'm struggeling with this problem. I have very simple (two threads) system, that wait for characters from usart. Everything work ok untill I turn on debug session. Then after a while it breaks it with known communicat ''Cannot access target. Shutting down debug session''

I recive characters using interrupts:

void USART1_IRQHandler (void)

{

  if(USART1->ISR & USART_ISR_RXNE) {

    msgBuffor[msgWritePtr++] = USART1->RDR;

    if (msgWritePtr > MESSAGE_BUF_SIZE) {

      msgWritePtr = 0;

    }

  }

}

Initialisation precedure:

void USART1_init(void)

{

  RCC->APB2ENR  |= RCC_APB2ENR_USART1EN;

  RCC->CFGR3 &= ~RCC_CFGR3_USART1SW;

  RCC->CFGR3 |= RCC_CFGR3_USART1SW_0;

  gpio_pin_cfg(TX_PORT, TX_PIN, GPIO_AF7_PP_50MHz);

  gpio_pin_cfg(RX_PORT, RX_PIN, GPIO_AF7_PP_50MHz);

  USART1->BRR = SystemCoreClock/115200UL;

  USART1->CR1 |= USART_CR1_TE | USART_CR1_RE |  USART_CR1_RXNEIE;

  USART1->CR1 |= USART_CR1_UE;

  NVIC_EnableIRQ( USART1_IRQn );

}

My findings so far:

- when no characters are received - problem does NOT appear,

- when interrupts are blocked obvieusly problem does NOT appear,

- it is not power issiue - checked with an oscilloscope

- CMSIS doesn't stuck in any fault handler procedure

- when run in normal mode both threads works properly (checked with LEDs)

- when debug session is stopped threads go further normaly

Any good idea is welcome

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    June 20, 2016
    Posted on June 20, 2016 at 23:41

    Assume it is not the code you have chosen to show..

    Using WFI anywhere?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..