STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Triggering ADC in Dual Mode with DMA - problems

Posted on December 21, 2016 at 05:41Hi,I(or may be ST) have a ptoblem. I tried to use ADC1 & ADC2 in regular dual mode with DMA on STM32F103C8T6 MCU(startup code generated by last CubeMX). If I configure ADCs in continues mode, then start ADC2(using...

Resolved! STM32L4 ADC Initialization Problem

Posted on July 15, 2016 at 14:35Hi All,I'm using STM32L475, STM32CubeMX 4.15.1, STM32L4 firmware library 1.5.1 and the code generated by STM32CubeMX. When initializing ADC1 and ADC2 the ADC2 initialization, MX_ADC2_Init(), sometimes calls ErrorHandl...

Resolved! STM32L4 ADC HAL Multimode

Posted on August 03, 2016 at 15:14Hello! I am trying to start ADC2 on stm32l476, but it always goes to error handler multimode.Mode = ADC_MODE_INDEPENDENT;     if (HAL_ADCEx_MultiModeConfigChannel(&hadc2, &multimode) != HAL_OK)     {     Error_Handl...

sttn by Associate
  • 1631 Views
  • 2 replies
  • 0 kudos

STM32F407 problem using DCMI with embedded sync (ITU656)

Posted on October 26, 2012 at 23:50I trying to use DCMI Interface connected to external video decoder IC ''TVP5150''. DCMI Interface is configured in Snapshot mode (single frame) and to use embedded data synchronization codes (ITU656) in ''Mode 1'' ...

rg256 by Associate
  • 3052 Views
  • 5 replies
  • 0 kudos

Resolved! Sdmmc incoming data not being seen, STM32L476, HAL - SOLVED

Posted on October 24, 2016 at 03:17 I'm working with STM32L476 trying to get a microSD card to communicate. Initially I'm sure I was getting a response, but now when I send CMD8 the chip does not see a respons from the card (SD_CMD_RSP_TIMEOUT)....

thmjpr by Associate II
  • 3620 Views
  • 4 replies
  • 0 kudos

Adding version number at hex file

Posted on November 16, 2016 at 08:58Hi,i'm using the STM32f4_discovery.Is there a way to include version number/Varible that i can read its value/string,when just viewing the file.maybe an executable that reads the hex file and locate the variable ?...

haukeye by Associate II
  • 6638 Views
  • 8 replies
  • 1 kudos

[BUG Report STM32_Cube_L4_1.5.1]SDMMC TX/TR DMA Dont work

Posted on September 19, 2016 at 15:29if one use sdmmc DMA for Tx AND Rx it will hang in HAL_SD_WriteBlocks_DMA or in HAL_SD_ReadBlocks_DMA in the modul stm32l4xx_hal_sd.c The reason is the DMA is enable in the first call of one of the routines and i...

Leo_Panda by Associate III
  • 1424 Views
  • 2 replies
  • 0 kudos

STM32F1 (stm32vldiscovery) - Can't make SPI work

Posted on January 12, 2017 at 15:27HelloI am trying to get SPI working on stm32vldiscovery.In my project I am using STM32 Peripheral Library (SPL), not HAL.For now I am trying to make SPI1 send data to SPI2, SPI2 echoes everything back to SPI1, and ...

Not able to program STM32l0476

Posted on January 13, 2017 at 02:14I am using lcd segment in my design. Before soldering LCD module, I am able to program my stm32l0476. But after soldering the LCD module, I am not able to do programming. Only dependency is TRACESWO (PA15 & lcd SEG...