STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 gpio clamping

Posted on January 14, 2017 at 14:30I have stm32 gpio pin connected through 5k resistor to the 12V supply. What voltage can I expect on the pin depending on the gpio configuration and processor model? Is there any internal clamping in the MCU?Do I ne...

stm32f303 opamp precision

Posted on January 14, 2017 at 20:38HelloIt is mentioned in the stm32f303vc that it's opamp GBW is 8, but as i measured in the lab, the opamp output (i tested opamp 1&2 in follower mode) can't follow a sine wave above 700KHz in frequency, i.e output ...

stm32f3 ADC input conflict with opamp output?

Posted on November 03, 2016 at 09:28I have a problem (I think) with PA6 in an STM32F303VCTx using it as an analog input. This pin is shared (along with other things) with opamp2_vout and even though I have not enabled any opamps, I think what I'm re...

Resolved! stm32f437xx.h

Posted on January 12, 2017 at 22:36Where can one find the current version of stm32f437xx.h?Thanks,jh

John Hite by Associate III
  • 2613 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F401RBT6 128KB Flash or 256KB

Posted on January 13, 2017 at 13:50Hello,I have a funny question. I have STM32F401RBT6 and my firmware is ~140KB in size. I can download it without any issues, but the datasheet for this chip says that it should have only 128KB of Flash?Also when I ...

srdjan by Associate II
  • 4258 Views
  • 8 replies
  • 0 kudos

Capturing image from SONY's image sensor

Posted on September 12, 2016 at 09:57I have made a board camera module using SONY's IMX225LQR-C image sensor. The following is its data sheet. I would like to ask a question about page 49 of this data sheet. http://astroccd.org/wp-content/uploads/20...

M. Jeong by Associate II
  • 3369 Views
  • 3 replies
  • 0 kudos

stm32f051 IAP problem

Posted on January 13, 2017 at 08:43Hi, Everyone.I am testing IAP on stm32f051.I made IAP code downloading from someone's IAP and did little modify.IAP code is located on 0x0800 0000 ~ 0x0800 2fff and application is located on 0x0800 3000 ~I wrote th...

paul0208 by Associate III
  • 2003 Views
  • 4 replies
  • 0 kudos