2016-09-30 3:50 AM
I am using a STM32L476 and I have a problem with de Vbus. It starts random to leak into de Vdd. I generate my code through CubeMX
Background: I am using a STM32L476JGY6. VDD-VDDA-VBAT-VDDIO2 running on 1V8VDDUSB running on 3V I noticed when I started my code there is a 50/50 change that the 1.8V Vdd voltage wil jump to 3-3.8VWhen this happens is see that there is no current flowing from or to my 1V8 power supply. And everything is drained from the 5V of the USB. When I remove the Vbus, it goes back to normalVbus from the USB is directly connected to the uC Vbus pin (E3) (like reference designs from STM)It only happens when I enable the Vbus sensing in the code through CubeMX. What i tried: - I added a delay before the USB starts to INIT but it doesn't help. - lower Vbus to a lower voltage (3V). Doen't help- Connecting USB after booting I will have this problem. When this happens, the USB starts to draw 80mA It seems the VBUS pin isn't 5V capable, also not after a stable Vdd. Can someone help me out? #vbus #current #stm32l476jgy6We’re moving the ST Community to a new platform to give you a better and more reliable community experience.