2016-09-27 3:26 AM
Hi there,
I build a Keil project for my STM32F103 MCU with STM32CubeMx.My goal is use the TIM1 channel 2 for control a Buzzer.I want to generate a PWM at 4KHz through TIM1 channel 2.I configured, with STM32CubeMx, the TIM1_Channel2 as ''PWM Generator CH2''.The problem regards the debug session. In particular, when I start the debug session and when the MCU executes the macro ''__HAL_AFIO_REMAP_TIM1_ENABLE()'' the debug session crash.Anyone have the same issue?Thanks!2016-09-27 4:37 AM
Hi fede.rico,
You should set the DBG_TIM1_STOP bit to debug a timer code. -Hannibal-2016-09-27 5:01 AM
I don't need to debug the timer code.
My problem regard the pin remap macro. At start up, the firmware initialise the the peripheral (auto-generated code) and when the code ''__HAL_AFIO_REMAP_TIM1_ENABLE() MODIFY_REG(AFIO->MAPR, AFIO_MAPR_TIM1_REMAP, AFIO_MAPR_TIM1_REMAP_FULLREMAP)'' in executed, the debug session crash.This is the problem.2016-09-28 7:46 AM
Hi fede.rico,
You would share the code ( part that contains the remapping) and .ioc file.-Hannibal-2016-09-30 3:03 AM
Hi,
I'm sorry but I can't share the code, I can add some pieces of code. This is the code for timer initialisation (generated by CubeMx):void HAL_TIM_MspPostInit(TIM_HandleTypeDef* htim)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(htim->Instance==TIM1)
{
/* USER CODE BEGIN TIM1_MspPostInit 0 */
/* USER CODE END TIM1_MspPostInit 0 */
/**TIM1 GPIO Configuration
PE11 ------> TIM1_CH2
*/
GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
__HAL_AFIO_REMAP_TIM1_ENABLE();
/* USER CODE BEGIN TIM1_MspPostInit 1 */
/* USER CODE END TIM1_MspPostInit 1 */
}
}
In particular, the debug session stuck on ''
__HAL_AFIO_REMAP_TIM1_ENABLE();''
This is the macro code:/**
* @brief Enable the remapping of TIM1 alternate function channels 1 to 4, 1N to 3N, external trigger (ETR) and Break input (BKIN)
* @note ENABLE: Full remap (ETR/PE7, CH1/PE9, CH2/PE11, CH3/PE13, CH4/PE14, BKIN/PE15, CH1N/PE8, CH2N/PE10, CH3N/PE12)
* @retval None
*/
#define __HAL_AFIO_REMAP_TIM1_ENABLE() MODIFY_REG(AFIO->MAPR, AFIO_MAPR_TIM1_REMAP, AFIO_MAPR_TIM1_REMAP_FULLREMAP)
I think that the problem is related to TIM1 pin remap.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.