STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Blink program does not run, GPIO pin shows 1.8v.

Posted on April 11, 2017 at 08:08I'm using stm32 cubemx with keil 5 to program simple blink on stm32f103c8 bluepill board with stlink/v2 i have configured pins RCC SYS and GPIOC  13 as output with 8 Mhz input frequency and HCLK is 72 MHz when I down...

0690X00000606j1QAA.png 0690X00000606h1QAA.png

RL-TCP Ping Problem

Posted on April 11, 2017 at 13:24The original post was too long to process during our migration. Please click on the attachment to read the original post.

ali2399 by Associate II
  • 1099 Views
  • 0 replies
  • 0 kudos

1Wire Driver implementation using STM32 Timer

Posted on April 10, 2017 at 11:50Hello, I'm using STM32L486 microcontroler and I have to implement eeprom 1Wire driver (DS2431). As first implementation, I used _NOP operation to generate 1�s Delay. It was working correctely and I was able to write ...

STM32F0 SPI DMA triggered by Timer compare match

Posted on April 06, 2017 at 20:25Hi!I have a question regarding the stm32f0 DMA engine. I am using an stm32f0discovery MB1034B evaluation board.I have the following setup:The SPI dma is configured to transmit 3 bytes from memory to the spi periphera...

STM32F0 - How to abort a DMA transfer?

Posted on April 09, 2017 at 21:57Hi!I was wondering what is the correct way to abort an ongoing DMA transfer?I have a situation where it seems like there was an incoming DMA request while I had the DMA disabled.I disable all channel triggers and whe...

I2C bus scanner

Posted on April 10, 2017 at 08:07Hi , I'm trying to make a inple I2C bus scanner ( re-writing simple arduino I2C scanner code )I am not sure how to return the error if there a device address exits?1st, am i trying to re-invent the wheel and there is...

benyBoy by Associate II
  • 5982 Views
  • 7 replies
  • 0 kudos

STM32L476RG + IDW01M1, delay problem

Posted on April 10, 2017 at 16:01Hi everyone,I was trying to send a message from a client to server using the standard code I got from CubeExpansionWifi. Before I send a second message I wait for an acknowledge from the server but this last one need...

STM+SD card+SPI interface

Posted on April 10, 2017 at 10:07Hello, I am trying to transfer data from BluePill STM32F103C8 to SD card using SPI protocol .Please give me suggestion about that....

Bug in stm32Cube v4.20.1

Posted on April 09, 2017 at 13:22Hi1. after project save flash latetny(RCC config page) become form X to 0 value2. can't select different data size for dma