User Activity

Posted on December 06, 2016 at 04:13I want to create the USB HID device function but I don't have any library or example code.Where to download the relation data for me reference?PS:I use a STM32F427 MCU.
Posted on November 25, 2016 at 09:35I have a slave device which is address 0x78 for write and address 0x79 for read.I want to confirm that why the below I2C transaction is difference?I want to reset the slave device and the mapping register informat...
Posted on November 16, 2016 at 06:27Hello!Sir:I have a project which is the MCU(STM32F427) to drive the camera module(OV5642) and referenced the arduino web site (https://github.com/ArduCAM/Arduino/tree/master/ArduCAM) to setup the register value fo...