cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4-Disco USB MSC HOST

tm3341
Associate II
Posted on August 05, 2014 at 18:51

Hello everyone.

I have a strange problem. Downloaded USB-Host-Device v2.1.0 library. I then started an example, set correct pinout for VBUS on F4-Discovery (PC0). USB MSC host works in FS mode. Everything is the same as in example, just FatFS by Chan is version 0.10b and pins are different. Then my example going like that:


/* Init Host Library */

USBH_Init( &USB_OTG_Core,

#ifdef USE_USB_OTG_FS

USB_OTG_FS_CORE_ID,

#else

USB_OTG_HS_CORE_ID,

#endif

&USB_Host,

&USBH_MSC_cb, 

&USR_Callbacks);


while
(1) {

/* Host Task handler */

USBH_Process(&USB_OTG_Core, &USB_Host);
 /* Device connected ? */

if
(HCD_IsDeviceConnected(&USB_OTG_Core)) {

//USBH_deviceOk = 0;

TM_DISCO_LedOff(LED_RED);

if
(i > 0xFF) {

/* Turn off LED */

TM_DISCO_LedOff(LED_GREEN);

}

/* Some counter */

if
(i > 0x7FFFF
/* && write*/
) {

i = 0;

/* Try to mount */

if
(f_mount(&fs, 
''''
, 1) == FR_OK) {

//if (f_mount(0, &fs) == FR_OK) {

err = f_open(&fil, 
''test_file.txt''
, FA_READ | FA_WRITE | FA_OPEN_ALWAYS);


if
(err == FR_OK) {

/* Append file */

f_lseek(&fil, f_size(&fil));

/* Put data */

f_puts(
''test string\n''
, &fil);


TM_DISCO_LedOn(LED_GREEN);

} 
else
{

sprintf(str, 
''Error code: %d\n''
, err);

TM_USART_Puts(USART6, str);

TM_DISCO_LedOff(LED_GREEN);

}

if
(write == 1) {

// Get volume information and free clusters of drive

err = f_getfree(
''0:''
, &fre_clust, &fss);

if
(err == FR_OK) {

// Get total sectors and free sectors

total = (fs.n_fatent - 2) * fs.csize / 2;

free = fre_clust * fs.csize / 2;


sprintf(str, 
''----------\nTOTAL: %d\nFREE: %d\n----------\n''
, total, free);

TM_USART_Puts(USART6, str);


write = 0;

}

}

/* Close file */

f_close(&fil);

}

/* Unmount */

f_mount(0, 
''''
, 1);

//f_mount(0, 0);

} 
else
{

}

i++;

} 
else
{

/* Not inserted, turn on RED */

TM_DISCO_LedOn(LED_RED);

TM_DISCO_LedOff(LED_GREEN);


write = 1;

} 

}

The problem is, that every USB stick is detected as inserted, but from my USBs the results are like that: USB 1: works always USB 2: works always USB 3: works only first write, then stop USB 4: sometimes recognized but could not open and mount. USB 4: sometime not recognized USB 4: sometimes recognized and worked I realize, that problem is in disk_read and disk_write of fatfs, because BUSY flag on read never stop. Do you know why is that?
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
daynial
Associate II
Posted on January 11, 2017 at 10:58

Can you please send me the complete project ? or send me the link 

Posted on January 12, 2017 at 10:40

Hi

khan.daynial

,

This is a very old thread. It should be better to start a new discussion for new request even if the topic is the same.This will be more easy for user forum to help/answer you.

So, I invite user forum to putting responses in your proper

https://community.st.com/0D50X00009XkfMvSAJ

.

Thanks

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen