STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LED blinking in assembler for STM32F103C8T6

Hello,I am trying small example LED blinking written in assembly only - see below. LED is placed to PB15. I am able to compile the program without error using this commands:arm-none-eabi-gcc -save-temps -nostdlib -nostartfiles -mcpu=cortex-m3 -ffrees...

JerryMC22 by Associate III
  • 2324 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F405 using dual USB host

Hi,I'm new to the ST32 world and would like to know if this is possible before I start experimenting with an STM32F405:Is it possible to use both USB interfaces as a USB host at the same time (only full speed and low speed, no high speed is required)...

Resolved! synching HRTIM's TIMA and TIMB

Trying to make a phase shift PWM for a DAB converter, i managed to do this exact functionality with normal TIM1 (Asynchronous mode), but im very very lost with HRTIM. I am able to produce complementary PWM signals for TIMA1 and TIMA2, and TIMB1 TIMB2...

Javier1_0-1739181617390.png Javier1_2-1739181348401.png
Javier1 by Principal
  • 2076 Views
  • 2 replies
  • 0 kudos

Resolved! Output Compare - STM32F3Discovery

Hello,I need to understand the implementation of using output compare with timers  as a basis to tackle a more advanced project. My start point/goal is a timer with a period of 3 seconds and it toggles when CNT equals 800ms(CCR1). Clock is running at...

Capture.PNG
daded.1 by Associate II
  • 1940 Views
  • 3 replies
  • 0 kudos

Two phase-shifted PUSH-PULL using HRTIM.

Hello! I am trying to implement a phase-shifting full bridge on the STM32F334 microcontroller using HRTIM. Two PUSH-PULL outputs and a phase shift between them, this is necessary for the LLC converter.I configured the master timer as an event source ...

APota.1 by Associate
  • 2009 Views
  • 1 replies
  • 0 kudos

Open bootloader for STM32H747 on USART

I want to use open bootloader on STM32H747 controller. I found that ST provides support for STM32H5 but not STM32H747. Can I use it for STM32H747? How can I port to my target controller?  

abasit by Associate
  • 803 Views
  • 1 replies
  • 1 kudos

PWM with shift phase and dead time, how to.

Hi,I am using the STM32G474 with HRTIM for the propose and also STM32CubeIDE.Is there any specific guide to make a four outputs (90 grades) PWM with dead time?The duty cycle must be changeable as well.I already read the relevant reference manual and ...

DKuro.1 by Associate III
  • 1359 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H533 ADC VDDA, VREF+ and input voltage range

I'm a little confused about the descriptions of the ADC VDDA, VREF+ and input voltage range.Do I understand it correctly thatVDD is the device supplyVDDA is the ADC supplyVREF+ is the ADC referenceIt says VREF+ can be supplied internally as 1.8 V, 2....

thansen by Associate III
  • 1857 Views
  • 2 replies
  • 1 kudos

STM32 NRST line

Hi,We are using STM32L452 for our project.We have problem with pin NRST.We set a 30K pull-up resistor (with pull-down capacitor of 0.1uF).Sometime voltage on the NRST pin is 3.3V and sometimes it is 1.4V.In cases it is 1.4V the MCU is stuck.We think ...

Ofer by Senior
  • 9574 Views
  • 11 replies
  • 3 kudos

STM32L073 LCD Controller

Just getting started with this uC and the ST toolset. I am trying to initialize the LCD controller but the init fails at:if (HAL_LCD_Init(&hlcd) != HAL_OK) {  Error_Handler(); }More specifically it times out at:  /*!< Wait Until the LCD Booster is re...

RSoen.1 by Associate III
  • 2966 Views
  • 6 replies
  • 1 kudos