User Activity

If I have a bare h753 MCU on my custom board. What connection in terms of communication peripherals and connectors do I need to achieve. Basically, I want to bootload the MCU. The next step is to be able to program, monitor, test simultaneously. From...
I have the main MCU serving as the master in the spi communication whose primary job is to transmit data over SPI lines to two slaves. If I choose hardware NSS signal configuration the IOC file assigns a default pin as the NSS signal for that SPIx pe...
I have a 12V GPIO high logic input on my board. Should I convert it to a 5V logic level or a 3.3V logic level? Previously, I have implemented 12V to 5V logic level conversion and already have components for this conversion in my inventory. If feasibl...
I have attached herewith the first iteration of the schematic for my custom stm32 board utilizing the H753ZIT6 MCU.I would like to clear few doubts regarding 1) In the nucleo schematic for the same, STM has used F7 MCU for their ST Link interface, sh...
Hi, I am designing for first time an RF PCB whose primary function is to convert incoming CAN Data and sent it over 2.4GHz frequency using an nRF24L01+ transciever. I am also incorporating an USB-B Micro for programming. As both have a different Impe...
Kudos given to