STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F031 uart bootloader write command

Posted on July 13, 2017 at 18:00I am using a STM32F031 micro and app note AN3155, using the built in UART bootloader on serial pins A9 and A10.  I wish to write sixteen bytes of zeros to an address near the start of flash, 0x08000010.  Referencing p...

0690X00000603wbQAA.jpg

Resolved! Bypass config for L476RGNucleo crashes

Posted on July 13, 2017 at 02:31Cannot get HSE Bypass to work for L476 Nucleo board, when 446RE Nucleo and F103RB Nucleo work fine.this stm32cubemx generated code spins in the _Error_Handler. Im thinking a bug in stm32l4xx_hal_rcc.c so far.  RCC_Osc...

Unterminated quoted string

Posted on July 13, 2017 at 16:58Hi, i'm setting up Eclipse with GNU ARM Cross Compiler.I made a simple Projekt ('blaccleds') with an STM32L0 Controller and the STM32L0xx_HAL_Driver-Package.I get the following Console-Output with an Error Message whe...

fff fff by Associate
  • 2274 Views
  • 3 replies
  • 0 kudos

Resolved! FIFO in UART of STM32F767

Posted on July 13, 2017 at 15:57Hello All,I wanted to know if the STM32F767, supports FIFO for the UART module? If yes, what is the size.I need the FIFO details for configuring the Hardware flow control.regards,Hemanth#uart #stm32f7 #fifo

STM32VLDiscovery st-link v2

Posted on July 13, 2017 at 16:05Hi,I know that the subject was already covered and concluded as st-link v1 has different hardware than v2 version.Just quickly looked into schematic and it seems that the MCU is the same as in v2 version (not v2-1). S...

dali Lighting Interface

Posted on July 13, 2017 at 11:38HiST has a DALI V1 library.Was this tested by DALI AG?Are there any plany to update it to DALI V2?Is there a ST third party offering a DALI V2 library?Thx