STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

uSD - DMA timeout in Write with new library

Posted on August 02, 2017 at 10:17Hello, the STM Community !I recently update all my libraries in my project, including the FatFS library, and the bsp_driver_sd.c.I also followed this page :https://community.st.com/docs/DOC-1546-cubemx-sdio-dma-fatf...

0690X00000607pKQAQ.png

I wanna get STM32F1xx Standard Peripheral LIB

Posted on August 01, 2017 at 12:25hi dear.I'm looking for  STM32F1xx Standrad Peripheral Lib old version.The version I want is V2.0.3 which came out in 2008.Can I get it from ST's website? or url link???

ikassma by Senior
  • 1201 Views
  • 8 replies
  • 0 kudos

STM32F0 generate signal on TIM3 with DMA

Posted on August 02, 2017 at 03:34Hi All,I am a newbie of STM32 developing. The board I am using is nucleo-f030R8. Right now I am trying to generate some pattern signals on timer3 like following waveform:An interrupt enables tim3, channel 1 will wai...

0690X00000603zVQAQ.jpg
Alex Z by Associate II
  • 818 Views
  • 0 replies
  • 0 kudos

USB CDC library for stm32f042k6t6

Posted on July 29, 2017 at 11:52Hello, I am trying to use stm32f042k6t6 MCU and I want to use the USB peripheral implemented in it. Could someone suggest me a USB CDC library I can use with this MCU to connect with PC, I am using the standard periph...

Resolved! ADC not scanning all channels

Posted on July 27, 2017 at 12:14Perhaps the title is wrong, but my code behaves like this: I have configured 4 channels to be converted in the ADC; I have put a variable which increments inside ADC irq EOC (EOC_Counter) and another which increments ...

ionutF by Associate III
  • 1648 Views
  • 2 replies
  • 0 kudos

STM32F334 embedded reference voltage

Posted on August 01, 2017 at 16:53Hello,Included attachement consists screen of internal reference parameters presented in datasheet.I think there is mistake because Vdd=31.8V seems not correct.I try to calculate how accurately can determine Vdda vo...

How to check from firmware whether SD card inserted in slot ?

Posted on July 31, 2017 at 18:48Hi, engineers. I am currently working on project, containing SD card. My HW is custom chinese board with STM23f407VET6 mounted and microSD slot connected to SDIO (proper pullup resistors seem to be in place). I made s...

vadim2 by Associate II
  • 4576 Views
  • 5 replies
  • 1 kudos

Resolved! HAL_SPI_TransmitReceive_DMA (STM32_FW_V1.7.0)

Posted on July 31, 2017 at 22:35In STM32Cube_FW_F7_V1.7.0/Projects/STM32746G-Discovery/Examples/SPI/SPI_FullDuplex_ComDMA example shows a simple DMA transfer with data cache on.  How can aRxBuffer buffer can be updated correctly without a region def...

How works the function HAL_SAI_Transmit_DMA()

Posted on July 26, 2017 at 09:58Hi Communities, can any body please explain me, how works exactly the function HAL_SAI_Transmit_DMA(). I am using STM32F746VGTX.This is one example:uint8_t TestArray[4] = {0x00,0xff,0x00,0x00};HAL_SAI_Transmit_DMA(hsa...