STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN RX FIFO overflow handling in STM32F4 FW package V1.16.0

Posted on July 27, 2017 at 20:20Hiho,we recently updated one of our projects to the newest Firmware package and had to realize that receiving CAN Messages per Interrupt did not work reliably anymore. We were able to track the problem down to the fac...

Blacbird by Associate II
  • 4014 Views
  • 4 replies
  • 0 kudos

Problem with RTC

Posted on August 07, 2017 at 10:54HelloI have a problem that I can not solve.This applies to stm32f072. I need to make a check if the processor has been powerless for more than 200ms at boot time. Trying to use RTC and backup registry with milliseco...

STM32 MCO1/2 Driving a second chip XTAL input

Posted on August 07, 2017 at 06:36Hello all,In my project, I'm using the STM32F411CEU6, with a 9.6MHz External TCXO as a clock source. I would like to use the same clock to feed another chip in the board.I was thinking of using the MCO1 or 2 in orde...

0690X00000607s0QAA.png
meir3 by Associate II
  • 2170 Views
  • 4 replies
  • 0 kudos

Is STM32 usable in this way?

Posted on July 13, 2017 at 12:49Dear sirs,I want to make drive recorder.I think to use, USB(Mass drive), SD card small, TFT window ,camera(I want many cameras).I do not want to make a proper product. I want only education or hobby.I found two produc...

USB OTG HNP and SRP Problem in STM32xxx

Posted on August 02, 2017 at 16:27Hello all,In USB OTG Driver SRP request after that USB_OTG_HandleSessionRequest_ISR invoking.What Need to be added to inform upper layer USB_OTG_HandleSessionRequest_ISR as per HAL Library?.  if (IsDeviceMode(&otgfs...

Resolved! Shouldn't HAL_TIM_IC_Start_IT() set TIMx->CCER?

Posted on August 06, 2017 at 18:48STM32L476-Nucleo board, with jumper wire from PA7 to PA0. Attempting to learn PWM Input Capture.GPIOA->AFR[0]:  0x20007701    00100000000000000111011100000001  PIN  0: TIM2_CH1  PIN  1:  -  PIN  2: USART2_TX  PIN  3...

Resolved! How to use HAL_HRTIM_IRQHandler

Posted on August 03, 2017 at 20:31Thank you for your patronage. I'm Japanese. I want to use Interrupt Service Routine(ISR) as shown in the picture below. So I want to use HAL_HRTIM_IRQHandler.I wrote the program as shown below, but I got an error. 

0690X00000607rqQAA.png 0690X00000607s5QAA.png 0690X00000607rkQAA.png
Ken Inoue by Associate III
  • 2415 Views
  • 2 replies
  • 0 kudos

RTC sub-second (RTC_SSR) issue

Posted on February 25, 2014 at 10:22Hi, I am having troubles with the subsecond register on stm32 I have a datalogger which logs data with a timestamp. I am doing multiple logs (~30) per second, so wanted to log sub-seconds as well. HOWEVER, as soon...

Freeze in eeprom

Posted on August 06, 2017 at 09:02hello.i use stm32f030p4. i use EEPROM emulation(save 20 byte) it's work until i add more code in my project.when the code Increase  Although I dont have any error in my code but program freeze in ee_init(); and i ha...

Resolved! STM32F10X DSP Library

Posted on July 03, 2017 at 09:23Hello, Can any one help me with STM32F10X DSP Library, Where and how can I get STM32F10X DSP Library.THANXXXX.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.