STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

External FLASH for F765 with the FMC

Posted on August 25, 2017 at 15:09Greetings All!In the past, we have used the F4 series (F427) with the FMC memory controller, to interface with 2GB of external NANDFLASH memory.  This worked with no problems.NOW, we have the same setup (same wiring...

LoRa Communication with STM32

Posted on August 23, 2017 at 13:15Hello everyone,I'm working on a LoRa project, using Murata's module ( stm32l082 & semtech's SX1276) , The aim of the project is to send some datas ( temperature, pressure .. ) to a gateway.I want to know if someone ...

Kim ElQ by Associate II
  • 8734 Views
  • 17 replies
  • 0 kudos

CSS is not triggering when HSE fails

Posted on April 25, 2017 at 09:21Hello,I'm using STM32F410RBT6 controller. I have configured it to use HSE with PLL (using cubeMX).I didn't soldered the quarts to the chip because i want to check that interruupt is generated when HSE fails and the C...

load2005 by Associate III
  • 2758 Views
  • 6 replies
  • 0 kudos

Resolved! Problems with ADC and dma

Posted on January 15, 2017 at 21:34  The original post was too long to process during our migration. Please click on the attachment to read the original post.https://community.st.com/s/question/0D50X00009XkdduSAB/triggering-adc-in-dual-mode-with-dma...

Ernesto B by Associate II
  • 2053 Views
  • 3 replies
  • 0 kudos

SPI slave bidirectional

Posted on August 25, 2017 at 12:09I have a difficulty with ST32F030 and Slave SPII'm trying to have it respond to an spi command:-Master sends 0x05, slave responds with an array of 7 bytes.It kind of works the first time, but then loses sync, and ge...

STM32F0308 USART set up

Posted on August 23, 2017 at 17:47 Hi, I am having trouble getting some basic USART up and running on the STM32F0308-DISCO board. I have tried both sending and receiving and don't seem to see anything coming through on either end. My code is as f...

Tom Power by Associate II
  • 6425 Views
  • 15 replies
  • 0 kudos

STM32F7 USB library supporting multi-packet mode

Posted on August 15, 2017 at 23:50Hi,I need high USB bandwidth in isochronous mode. The STM32F7 is powerful but the bandwidth depends on how the USB packet management is done.Is there a plan to support multi-packet mode in the HAL/lib/driver that co...

Resolved! STM32L433 - No JTAG Devices Found

Posted on August 23, 2017 at 22:13I'm using an ARM-KEIL ULINKPro debugger on a custom board using the STM32L433 processor. There's a JTAG connector on the board, and I'm using a TC2050-IDC-050 20:10 cable from Tag-Connect, which was recommended by t...