STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MCU selection problem

Posted on September 07, 2017 at 09:54Hello. sirI am going to make a prototype so that I can use some sensors(3ea, 2 I2C, 1 UART)and read the measured values to the mono LCD(3~4line), In addition, Bluetooth can be used.Product development is determin...

What is the difference between CMSIS and CMSIS-RTOS?

Posted on September 07, 2017 at 08:45I can remember few years ago, we could create projects with CMSIS library. But nowadays when I search about CMSIS, there is CMSIS-RTOS instead of that. Is it mean we should use CMSIS-RTOS from now? Also I am conf...

m m by Associate II
  • 8649 Views
  • 3 replies
  • 0 kudos

Continous UART/DMA receiver stops within STM32F0x

Posted on September 04, 2017 at 09:16Hello,I had a problem with my UART interface on STM32F091RC. I have seen that others encountered the same, but I am not able to fix yet in my side.I have UART Rx and Tx in DMA normal mode.Tx function is working f...

How is OSC_OUT connected at HSE bypass source mode?

Posted on September 07, 2017 at 05:24There are two different descriptions in AN2586 and AN1709.In AN2586 it says it must be left highZ, and as far as I can tell from the figure it means floating.In AN1709 it says it should be tied to ground.Does the...

T YX by Associate
  • 849 Views
  • 0 replies
  • 0 kudos

STSW-LINK009 install

Posted on September 06, 2017 at 09:21HiI have one set ' P-NUCLEO-53L0A1 '.It includes: STM32F401 and X-NUCLEO-53L0A1I download STSW-LINK009 from http://www.st.com/en/development-tools/stsw-link009.html And run the stlink_winusb_install.bat with admi...

Wu Thomas by Associate II
  • 3839 Views
  • 4 replies
  • 0 kudos

STM32F407 Discovery fsmc lcd problem

Posted on September 05, 2017 at 20:33I am trying to use fsmc to control my lcd display, but I can't init lcd from my code. I configured fsmc as lcd interface memory type in CubeMx, but there is something wrong with reading registers value, when I'm ...