STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is hardfault?

Posted on September 07, 2017 at 18:02I want to know more about hardfault.1-)Is there any documentations about hardfault on stm32f415 microprocessor?2-)Why does Hardfault occur(all reason)?3-)Are there any difference between the processors(for exampl...

four uarts on stm32L433?

Posted on September 05, 2017 at 22:05Is it possible to get four USART/UART devices at once on the STM32L433 in a 64-pin package? I need one UART for input, one for output, one for external logging, and USART1 for debugging.Is this doable? I've used ...

Square wave generation with STM32 and timer

Posted on September 06, 2017 at 22:27hi everyone,I'm trying to generate a square wave / quadrature signal ( 2 square wave with 90 degrees offset). The board is a STM32F103C8The goal of the project will be to send an exact number of pulse. Frequency ...

paul sauv by Associate III
  • 1823 Views
  • 1 replies
  • 0 kudos

STM32F769IIT Development environment

Posted on September 07, 2017 at 13:54I am looking for some guidance in choosing a development environment and compiler for the STM32F769IIT chip.  This is my first venture into the ARM world.  I have been programming Microchip parts for about 25 yrs...

pmuldoon by Associate
  • 717 Views
  • 0 replies
  • 0 kudos

FT6236 interfacing with I2C3 inside STM32F407

Posted on August 28, 2017 at 09:53Hi,     I m using FT6236 capacitive touch screen controller with I2C3 inside STM32F407. All required Connections have been checked thoroughly. I have referred the reference code from all possible links available fro...

24C02 with STM32CubeMX

Posted on August 25, 2017 at 13:11Hello,I'm trying to use this code to write/read a EEPROM 24C02,but it's not working,what i'm doing wrong?Could someone post a example please?uint8_t eedget[1],eedata[1];void main(){eedata[0] = 0x01;eedata[1] = 0x02;...

STM32L4 series PLLs?

Posted on September 04, 2017 at 20:27There seems to be something I don't quite get.In the reference manual it says 'The PLLs input frequency must be between 4 and 16 MHz.' and 'The selected clock source is divided by a programmable factor PLLM from ...

MCU selection problem

Posted on September 07, 2017 at 09:54Hello. sirI am going to make a prototype so that I can use some sensors(3ea, 2 I2C, 1 UART)and read the measured values to the mono LCD(3~4line), In addition, Bluetooth can be used.Product development is determin...