STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C busy flag is always set. (without library)

Posted on September 13, 2017 at 15:26MCU : STM32F405I wish to use I2C without library.But, I got always busy flag on I2C_SR2 register---------------------------------------------------------------------------void set_gpio_af_i2c(){ RCC_AHB1ENR |= GP...

0690X00000608AEQAY.png

Does STM32F4xx support UART IAP?

Posted on August 03, 2015 at 05:09Hi Guys, I download sample code for UART IAP(AN4657) and try to use on my STM32F405, but till now I havn't made it run.and I found below info from document:Content•  STM32L0 HAL Driver 1.2.0. file:///D:/dev/gogo-lit...

dqyang by Associate II
  • 2225 Views
  • 6 replies
  • 0 kudos

Resolved! Can SPI hardware control hold NSS low for a multiple byte frame?

Posted on September 13, 2017 at 22:08I've got a STM32L476 with a SPI port configured as a master, talking to a single slave device. The slave device needs to communicate in 32-bit frames, with the chip select held low for the entire frame. Is there ...

kotwal by Associate II
  • 1567 Views
  • 2 replies
  • 0 kudos

STM32CubeMX FATFS + USB-MSD

Posted on September 13, 2017 at 21:23I’m trying to implement a simple data-logger that runs on a bespoke STM32F2xx board which is capable of storing data to an SD-Card (SDIO 4-bit + DMA) and will enable windows to copy the stored data from the SD-...

GnR by Associate II
  • 931 Views
  • 0 replies
  • 0 kudos

Resolved! LL driver support from STM32Cube

Posted on September 12, 2017 at 18:46Hello,I was looking to import LL driver for my STM32L053 device. I see user manual for  STM32F4 LL driver. I wanted to know if we have LL code generation support in STM32CubeMX for STML0xx family?Thanks,Harsha

Jagadish by Associate II
  • 2269 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F446 SPI transfer bit width

Posted on September 12, 2017 at 19:57IMO, *to* is inappropriate here - as far as I can see, transfer width in 'F446's SPI can be only 8-bit *or* 16-bit.JW

0690X00000608CTQAY.png

SPI + DMA receive only on STM32F4

Posted on September 13, 2017 at 16:56In my situation, I need to do SPI receiving with DMA (master side), and not care about Tx. I have three choices in the STM32Cube: Full-duplex masterHalf-duplex masterReceive only masterAnd I have two choices for...