User Activity

Has anyone got the Adafruit 1.8" Color TFT Shield to work with a Nucleo H743?I have tried the demonstration program from the STM32Cube_FW_H7_V1.3.0 package that supports this board, but nothing is displayed. I have verified that SPI data is being sen...
Posted on May 22, 2017 at 15:35The STM32L471 Errata document states that:  An overconsumption can appear on VDDA in the following conditions:• a voltage VPAD is applied on PA3 or PB0 with VDDA+ 50 mV < VPAD < VDDA + 600 mV ...Our application uses ...