STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I use stm32f407 for smartcard project ?

Posted on September 18, 2017 at 11:06Hi, Can I use stm32f407 for smartcard project ? I found prepared smartcard project for some EVAL boards and STM32L053 boards in st's website. I wonder that can stm32f407 be used instead of eval boards and l053 bo...

Resolved! display address CCM

Posted on September 15, 2017 at 17:52Hi,I try to move some array in CCM on stm32f415.I modify the ld script with  CCM_SRAM   (rwx) : ORIGIN = 0x10000000, LENGTH = 64K .ccmram : { . = ALIGN(4); _sccmram = .; /* create a global symbol at ccmram start ...

OA1ZHA / TSZ121 precision amplifier

Posted on September 16, 2017 at 12:33I'm not sure if I'm understanding the gain bandwidth correctly, but can I use OA1ZHA op amp for a signal with ADC sampling frequency of 2 kHz? or am I really limited to only 400 kHz based on maximum gain bandwidt...

0690X000006045dQAA.jpg
Kevin A by Associate
  • 1242 Views
  • 1 replies
  • 0 kudos

Output control Question

Posted on September 18, 2017 at 02:59EX) ODR = 1   -> I/O Pin State = 0 ?It is True?If ODR = 1 then I / O port is also 1?Is it OutputControl Not Gate?

0690X00000608HJQAY.png

Update from F4 to F7 -> Performance Problems

Posted on September 15, 2017 at 14:17Hallo everybody,i have a circuit board whitch is fitted with a STM32F429BIT.The Software use STemWin and LWIP (without RTOS) and works good.Now i has order the same circuit board with the pin compatible STM32F767...

mfrank9 by Associate III
  • 784 Views
  • 1 replies
  • 0 kudos

Bootloader + Two applications

Posted on September 07, 2017 at 08:19Hi, I have to download second application and enter second application from the first application.Bootloader to First application jump is happening and working fine.I have problem to jump to second application fr...

Resolved! Maximum output current value of PWM, TIM

Posted on September 16, 2017 at 18:18Sorry for my poor English.What is the maximum output current value of PWM using TIM? Where can I find it in the data sheet? I am using STM32F334. I am investigating whether the MOSFET can be directly driven by th...

0690X00000608GvQAI.png
Ken Inoue by Associate III
  • 2014 Views
  • 4 replies
  • 0 kudos