STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FMC LTDC SDRAM Burst access

Posted on September 21, 2017 at 11:46Hi guys,i have a custom board on which both, LTDC and FMC conneted SDRAM, is used.If I enable the burst access to the SDRAM the board crashes after a while. Assuming the accesses between SDRAM and LTDC are not ha...

FMC config in STM32L4

Posted on September 20, 2017 at 13:37I am trying to configure STM32L4 with an 8-bit monochrome LCD using FMC using CubeMx Tool. I have configured the timing parameters. I could see that the LCD Command and Data are to be written in a particular addr...

Anand A by Associate III
  • 1594 Views
  • 3 replies
  • 0 kudos

Resolved! Cannot connect to STM32F469 CPU

Posted on September 20, 2017 at 13:06Hi,I'm trying to setup our new PCB with a STM32F469IGH6 MCU.Our software includes a RealTime OS and some User Defined Modules as Testsoftware.The Firmware formerly was written for the STM32F469 Discovery Board an...

STM32F051 programming issue

Posted on September 12, 2017 at 12:59Dear Community,I noticed a strange problem while attempting to program a STM32F051 device. The device is part of a larger circuit and gets its supply voltage from a 3.3V LDO regulator and the VDDA is supplied by ...

0690X00000608BzQAI.png
jogerh by Associate II
  • 2020 Views
  • 3 replies
  • 0 kudos

External interrupt react on rising edge only

Posted on September 20, 2017 at 15:29Hi everybody.I am playing with stm32f411 and external interrupts. I have trouble with interrupt calling in the moment i need. Could you please take a look at my issue?Id like to call the interrupt by user button ...

STM32L100xx USART Smartcard Mode

Posted on September 20, 2017 at 12:31So recently I had to dig in and fix some code about the USART in SmartCard mode. Apparently each byte i send is echoed back at me, triggering the RXNE. My question is do I get the RXNE before the TC of the byte I...

Nucleo-H743ZI Support files lacking DXF

Posted on September 19, 2017 at 18:24Was just notified the Nucleo-H743ZI board would be shipped but when I downloaded the support files I found no support for building a shield. The CAD files were there but in binary export not ASCII, not everyone o...

KevinA by Senior
  • 791 Views
  • 2 replies
  • 0 kudos