STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F091CCU6 Controller

Posted on September 26, 2017 at 07:54Hi All,I used 'STM32F091CCU6' this controller.Can I Implement OTA in this controller.  Please give me soluation as soon as possibleRegardsNitin Kanani#stm32f091 #stm32ff103 #stm32f091ccu6 #stm32f

STM32Cube does not run

Posted on September 25, 2017 at 22:10I just installed STM32CubeMX on my Windows 10 machine.  When I try and launch it, I get the following error.  How can I fix this?  I have Java installed- for many environments and the Java About returns the messa...

0690X00000608NIQAY.png 0690X00000608NlQAI.png
ttatakis by Associate III
  • 1209 Views
  • 3 replies
  • 0 kudos

Resolved! STemWin problem: EDIT text bug

Posted on September 25, 2017 at 21:42I've got a bug with the text of the Edit box. It show's strange chars or drawings, maybe another language font. I'm using the emwin with the SSD2119 driver. All other fixed texts and labels are correct (see the a...

STM32L4 USB VCP Receive Buffer Issue

Posted on September 25, 2017 at 19:41Hi,I am using STM32L4 Discovery board, I have generated USB VCP code from cube MX and configured as CDC class in Device mode. I am facing an issue with Receive buffer, I don't understand the issue. If host send d...

Sunny T by Associate
  • 1498 Views
  • 2 replies
  • 0 kudos

A suggestion for a new register in STM32 processors

Posted on September 25, 2017 at 20:17When using watchdog timers, the processor resets when your program fails to clear the watchdog timer within a predetermined period. The RCC_CSR has two bits that can be queried at boot time that indicate a watchd...

gdb client exectuable path for Segger JLink

Posted on September 25, 2017 at 19:28Hi all,I'am working on a project with System Workbench for STM32.Does anyone of you know what the absolute path is for the gdb client executable, when using Segger JLink debug /programming adapter? Where can I fi...

Max Veen by Associate II
  • 636 Views
  • 0 replies
  • 0 kudos

STM32 DFSDM - simultaneous sampling of multiple channels

Posted on September 25, 2017 at 15:11I am a bit confused about the capabilities of the STM32 DFSDM module. The documentation says (section 17.3.77) that the channels selected for are converted one after another, but is it possible to sample multiple...