2017-05-17 9:24 AM
I want to activate the LSE clock on STM32L1 board using processor stm32l152xe on Nucleo board. board
version MB1136 C-03. I far as I can tell no hardware changes required to get the LSE to work.
My plan is to run the real time clock externally that interrupts TIM9 for accurate measurements.
DO I have to see high voltage (3.3 volts) at the output of the Port C pin 15 (PC15), for the LSE crystal to operate properly on STM32L1 Nucleo board? I was not able to see the voltage going high at that pin.
I have initialized the system clocks as follows:
void
SystemClock_Config(
void)
{
RCC_ClkInitTypeDef
RCC_ClkInitStruct = {0};
RCC_OscInitTypeDef
RCC_OscInitStruct = {0};
/* Enable HSI Oscillator and Activate PLL with HSI as source */
// RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.
OscillatorType
= RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE
|RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.
LSEState
= RCC_LSE_ON;
RCC_OscInitStruct.
HSIState
= RCC_HSI_ON;
RCC_OscInitStruct.
HSICalibrationValue
= RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.
MSIState
= RCC_MSI_ON;
RCC_OscInitStruct.
MSICalibrationValue
= 0;
RCC_OscInitStruct.
MSIClockRange
= RCC_MSIRANGE_5;
RCC_OscInitStruct.
PLL
.
PLLState
= RCC_PLL_ON;
RCC_OscInitStruct.
PLL
.
PLLSource
= RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.
PLL
.
PLLMUL
= RCC_PLL_MUL6;
RCC_OscInitStruct.
PLL
.
PLLDIV
= RCC_PLL_DIV3;
if
(HAL_RCC_OscConfig(&RCC_OscInitStruct) !=
HAL_OK)
{
Error_Handler();
}
/* Set Voltage scale1 as MCU will run at 32MHz */
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/* Poll VOSF bit of in PWR_CSR. Wait until it is reset to 0 */
while
(__HAL_PWR_GET_FLAG(PWR_FLAG_VOS) !=
RESET) {};
/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
clocks dividers */
RCC_ClkInitStruct.
ClockType
= (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.
SYSCLKSource
= RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.
AHBCLKDivider
= RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.
APB1CLKDivider
= RCC_HCLK_DIV1;
RCC_ClkInitStruct.
APB2CLKDivider
= RCC_HCLK_DIV1;
if
(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) !=
HAL_OK)
{
Error_Handler();
}
}
The TIM9 clock is initialized as follows:
void
rtimer_arch_init_external(
void)
/* TIM9
init
function *///static void MX_TIM9_Init(void)
{
TIM_ClockConfigTypeDef
sClockSourceConfig;
TIM_IC_InitTypeDef
sConfigIC;
TIM_SlaveConfigTypeDef
sSlaveConfig;
TIM_MasterConfigTypeDef
sMasterConfig;
htim9.
Instance
= TIM9;
htim9.
Init
.
Prescaler
= 0;
htim9.
Init
.
CounterMode
= TIM_COUNTERMODE_UP;
htim9.
Init
.
Period
= 0;
htim9.
Init
.
ClockDivision
= TIM_CLOCKDIVISION_DIV1;
if
(HAL_TIM_Base_Init(&htim9) !=
HAL_OK)
{
Error_Handler
();
}
sClockSourceConfig.
ClockSource
= TIM_CLOCKSOURCE_ETRMODE2;
sClockSourceConfig.
ClockPolarity
= TIM_CLOCKPOLARITY_NONINVERTED;
sClockSourceConfig.
ClockPrescaler
= TIM_CLOCKPRESCALER_DIV1;
sClockSourceConfig.
ClockFilter
= 0;
if
(HAL_TIM_ConfigClockSource(&htim9, &sClockSourceConfig) !=
HAL_OK)
{
Error_Handler
();
}
sMasterConfig.
MasterOutputTrigger
= TIM_TRGO_RESET;
sMasterConfig.
MasterSlaveMode
= TIM_MASTERSLAVEMODE_DISABLE;
if
(HAL_TIMEx_MasterConfigSynchronization(&htim9, &sMasterConfig) !=
HAL_OK)
{
Error_Handler
();
}
if
(HAL_TIM_IC_Init(&htim9) !=
HAL_OK)
{
Error_Handler
();
}
if
(HAL_TIMEx_RemapConfig(&htim9, TIM_TIM9_LSE) !=
HAL_OK)
{
Error_Handler
();
}
sConfigIC.
ICPolarity
= TIM_INPUTCHANNELPOLARITY_RISING;
sConfigIC.
ICSelection
= TIM_ICSELECTION_DIRECTTI;
sConfigIC.
ICPrescaler
= TIM_ICPSC_DIV1;
sConfigIC.
ICFilter
= 0;
if
(HAL_TIM_IC_ConfigChannel(&htim9, &sConfigIC, TIM_CHANNEL_1) !=
HAL_OK)
{
Error_Handler
();
}
st_lib_hal_tim_clear_flag(&htim9, TIM_FLAG_UPDATE);
/* Enable TIM10 Update interrupt */
st_lib_hal_tim_enable_it(&htim9, TIM_IT_UPDATE);
st_lib_hal_tim_enable(&htim9);
st_lib_hal_nvic_set_priority((st_lib_irq_n_type)
TIM9_IRQn, 0, 0);
st_lib_hal_nvic_enable_irq((st_lib_irq_n_type)(
TIM9_IRQn));
}
Thanks.