User Activity

Hi ,I'm doing an audio recording with the SAI interface of the STM32L4R9AI microcontroller.I'm using DMA in circular mode and I'm getting audio data which I wrote into SD memory.However, when I tried to open the recorded file , I hear my audio speec...
Posted on November 22, 2017 at 21:05Hi,I'm required to integrate FatFs file system on my raw NAND flash memory. I'm interfacing the NAND through SPI peripheral of the STM32L486RG microcontroller. I have developed NAND a low level driver through whic...
Posted on November 20, 2017 at 12:13Hi, I'm working on a project using STM32L486RG microcontroller and using IAR 8.11 workbench IDE.Within this project , I'm required to interface Micron raw NAND flash memory through SPI peripheral and integrate FAT...
Posted on December 13, 2016 at 15:36Hi, I'm working with STM32L486RG ultra low power microcontroller using the IAR v7.4 IDE.I'm using the RTC peripheral in order to get the real time clock . My clock source is an LSE crystal which has 32768Hz as fre...
Posted on December 06, 2016 at 11:44Hi, I'am working on STM32L486RG MCU and I'am using RTC to get the real time value.I know that ST provides 2 RTC format for the time : the RTC_FORMAT_BIN and RTC_FORMAT_BCD ( as defined in the HAL ). I know the dif...
Kudos from