STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476 CAN RX interface (FIFO capacity)

Posted on October 23, 2017 at 10:16Hello to every one,could anyone clarify something about the capacity of every FIFO stage description?At datasheet main features, in reception part, there is a:'Two receive FIFO with 3 stages'Which is the capacity o...

STM32L152 wrong time period of the pwm signal!

Posted on October 19, 2017 at 15:17 Hello I use the STM32l152RCT6 Discovery-Board. I use the PWM over the DMA. Everything works well! But if I call my functionvStartDMA() with the PWM values 0xFF and 0x00 the result of the pwm pulses are wrong...

0690X00000608hmQAA.png
sommer2 by Associate II
  • 2665 Views
  • 3 replies
  • 0 kudos

STM32F407 HS MSC read\write speed

Posted on August 08, 2012 at 15:37HI, I did connect STM32F407DESCOVERY to SMSC USB3320 ULPI (USB High Speed mass storage configuration). And uSD curd via SDIO interface. The MCU configured to work in its maximum performance: CPU clk 168Mhz , Enpoint...

Example programs for USB on Nucleo?

Posted on October 23, 2017 at 09:41Hi allWe have an STM32 Nucleo-64 board, model NUCLEO-L476RG. We try desperately implementing an USB device with this card. We are using STM32CubeMX and MDK-ARM toolchain (Keil uVision5). We have load STM32CubeL4 Fi...

helene by Associate II
  • 1037 Views
  • 1 replies
  • 0 kudos

ST-LINKv2 not working fine after updating

Posted on October 23, 2017 at 09:51Hi guys, I'm new here and I need some help if possible. I have some trouble with ST-LINK v2 device. I'm using MacBook Pro with Bootcamp running Win 10. When I start st-util from macOS console everything works fine,...

Saving variables to non volatile memory in STM32F429

Posted on October 20, 2017 at 20:33 I have been reading so many post related to saving data to non volatile memory in STM32F4, but until now I haven't had success. I wonder if you can help me by doing this? Modifying my scatter file I have: LR...

is it available to get 9MHZ PWM from STM32F334

Posted on October 21, 2017 at 10:58Hi ST,my purpose is  to use STM32F334 to output 9MHZ PWM ,and need to adjust the pulse width each period by the burst DMA of the chip, is it available ? thanks

J L by Associate II
  • 2085 Views
  • 8 replies
  • 0 kudos

unable to erase or programming

Posted on October 21, 2017 at 16:09Hi,I have mounted on my board a STM32F030C8. I flashed passed versions of projects: all ok. But when I flashed the last version nothing is  possible to do: message are: 'no target connected' and 'error: flash erase...

sav gas by Associate II
  • 1533 Views
  • 2 replies
  • 0 kudos