cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 Cube FW Library's SPI bug

just4you
Associate III
Posted on June 30, 2017 at 04:40

F0 cube library's SPI API has problems.

In spite of running 8 bit transmission mode, the library transmit a 16 bit data.

So the misalignment check routine does not filter the unaligned address on 8 bit mode.

Then, I think this 8 bit transmission code does not communicate with 16 bit transmission,

the way F4 cube library works.

It's not welcome method, because user can not expect inside 16 bit transmission of the SPI API functions.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on July 03, 2017 at 16:43

Hi

Whang.Se_Hee

,

I think your are using an old STM32CubeF0 version, asthis limitation is fixed within the STM32CubeF0 firmware package V1.8.0 (available since 07-April-2017)

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen