STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to get SWO working with STM32CubeMX-generated Makefile?

Posted on November 10, 2017 at 13:29Hello,I am using the arm-eabi-none- toolchain on Mac OS X 10.11 using STM32CubeMX 4.22.1 to create the initialization code, a Makefile that I wrote and the ST-Link/v2 for programming.  With that environment, I can...

pgregson1 by Associate III
  • 1762 Views
  • 4 replies
  • 0 kudos

Issues using USB MSC Host Libraries

Posted on November 10, 2017 at 16:28I have recently added USB support to a product, using the STM32_USB_Host_Library MSC class taken from the STM32Cube_FW_F2_V1.7.0 examples.We successfully detect devices and write and read from the disk until we ge...

How do I configure Memory Protection Unit?

Posted on November 03, 2017 at 19:56How do I configure the Memory Protection Unit in STM32F103RB? I need to protect a region of memory from writing. Can I do it using MPU?#memory-protection #stm32f103xx #cortex-m3 #cortex-m4

Cortex-M3 Memory Protection Configuration(MPU)

Posted on November 12, 2017 at 17:55 I want to protect a memory region from writing. I've configured MPU, but it is not generating any faults. The base address of the region that I want to protect is 0x20000000. The region size is 64 bytes. He...

Resolved! Why can't i connect to my STM32F103

Posted on November 08, 2017 at 15:28I have a ST-LINK-V1 connected to a OLIMEXINO-STM32, an F103RBT6 using the System Workbench.Using the ST-LINK utility I can see that I communicate to the ST-LINK. I can flash the com light and change basic configur...

Write and read FLASH STM32F4

Posted on November 13, 2017 at 11:21I make a simple code to write and read data from address,show as below. But always get message 'Cannot access target' from keliC. EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS; EraseInitStruct.VoltageRange =...

tan loi by Associate II
  • 868 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F4 FLASH One-Time programmable (OTP)

Posted on November 12, 2017 at 16:57I make a simple project to write and read data from FLASH OTP. I checked states of 16 blocks in OTP , have 3 block is block (state 0x00) and i write to other block with state 0xff. But i just correct only 1 times,...

tan loi by Associate II
  • 2397 Views
  • 2 replies
  • 0 kudos

Hello folks I am recently started using stm32 boards

Posted on November 12, 2017 at 23:21hello folks i am trying to output on a of my nucleo F44RE board i am using STM32CUBE and ewarm problem is when i connect a scope to the pin i dont detect anything would anyone know why this is my code i am trying ...