cancel
Showing results for 
Search instead for 
Did you mean: 

ws2812 with multiple output

mahmoud boroumand
Associate III
Posted on July 24, 2017 at 13:38

Hello

i use stm32f103c8 and use this library 

https://github.com/g4lvanix/0xWS2812

  .it work without any problem in all pin(16 pin) of gpio.but it work on only one of the port (gpioa-gpiob) and i can olny use one of the port and 16 out put but i need 32 output.how can use two port at the same time?
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on July 24, 2017 at 13:49

You can't. Use a second timer with suitable DMA channels.

JW

Posted on July 24, 2017 at 16:13

Asked and Answered

https://community.st.com/0D50X00009XkXm1SAF

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..