STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power LoRa disco board external

Posted on July 05, 2017 at 14:32 Have been playing with the B-L072Z-LRWAN1 and it all works fine. Now we would like to hook up directly to the Murata ABZ (via the break out / CN2 and CN3). As a start I have externally powered the ABZ. I expected ...

Resolved! STM32F105 flash erase problem

Posted on June 16, 2017 at 16:56Hello!Got a weird problem with STM32F105R8T6 chipWhile the same code, compiled and running on  STM32F103R8T6, works okProgram size is 17 kB as can be seen from map file:AHBPrescTable 0x0800473a Data 16 system_stm32f1x...

yury by Associate II
  • 2669 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L476G-Disco LSE Startup Problem

Posted on January 05, 2018 at 14:44Hi everyone,I want to use RTC module and LSE crystal which is default on board 32768KHz. I generate the code via STM32Cube because I couldn't find any example of RTC that used via LSE. After generated, the code doe...

STM32L431 Flash reading problem

Posted on January 09, 2018 at 11:43Hello,I have a problem with my bootloader. At the first launch I write a 64 bit word in flash in 0x8004030. I was able to check with J-Mem to make a dump of the memory and it flash writing OK.If I read the value at...

eric2 by Associate
  • 612 Views
  • 0 replies
  • 0 kudos

putty terminal text colour change

Posted on January 08, 2018 at 22:39trying to change the colour of the text on the usart what is the correct combination to use?<p>send_usart(0x1B); send_usart('['); send_usart(3); send_usart(4); send_usart('m');</p>

j g by Associate II
  • 1381 Views
  • 2 replies
  • 0 kudos