stm32l053 adc multiple channel without DMA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-09-05 5:24 AM
Hi,
I'm trying to read 2 number of ADC channels on stm32l053 without DMA by initializing channel 1, reading & deinitializing channel 1 then
initializing channel 2, reading & deinitializing channel 2.
I can read ADC count, but both the values are similar.
Is there any way i can use ranks (like it is used in stm32f0's) in stm32l053 to convert multiple channels without using DMA?? & I've posted my init, deinit codes for your consideration, if anything i was missing please suggest me the way out.
Thanks in advance.
/* ADC init function */
void MX_ADC_Init(int ch)
{ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc.Instance = ADC1; hadc.Init.OversamplingMode = DISABLE; hadc.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV1; hadc.Init.Resolution = ADC_RESOLUTION12b; hadc.Init.SamplingTime = ADC_SAMPLETIME_239CYCLES_5; hadc.Init.ScanDirection = ADC_SCAN_DIRECTION_UPWARD; hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc.Init.ContinuousConvMode = DISABLE; hadc.Init.DiscontinuousConvMode = DISABLE; hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIG_EDGE_NONE; hadc.Init.DMAContinuousRequests = DISABLE; hadc.Init.EOCSelection = EOC_SINGLE_CONV; hadc.Init.Overrun = OVR_DATA_PRESERVED; hadc.Init.LowPowerAutoWait = DISABLE; hadc.Init.LowPowerFrequencyMode = DISABLE; hadc.Init.LowPowerAutoOff = DISABLE; HAL_ADC_Init(&hadc);/**Configure for the selected ADC regular channel to be converted.
*/ if( ch == 0 ){ sConfig.Channel = ADC_CHANNEL_0; }else if ( ch == 1){ sConfig.Channel = ADC_CHANNEL_1; } HAL_ADC_ConfigChannel(&hadc, &sConfig); if (HAL_ADCEx_Calibration_Start(&hadc, ADC_SINGLE_ENDED) != HAL_OK) { /* Calibration Error */ // Error_Handler(); }}void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc){GPIO_InitTypeDef GPIO_InitStruct;
__GPIOA_CLK_ENABLE(); __ADC1_CLK_ENABLE(); GPIO_InitStruct.Pin = GPIO_PIN_1; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);}
void HAL_ADC_MspDeInit(ADC_HandleTypeDef* hadc)
{/* USER CODE BEGIN ADC1_MspDeInit 0 */
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_0); HAL_GPIO_DeInit(GPIOA, GPIO_PIN_1);__ADC1_CLK_DISABLE();
__GPIOA_CLK_DISABLE(); /* USER CODE BEGIN ADC1_MspDeInit 1 *//* USER CODE END ADC1_MspDeInit 1 */
}
#stm32l053 #adc- Labels:
-
ADC
-
STM32L0 Series