cancel
Showing results for 
Search instead for 
Did you mean: 

Icube_LRWAN ( End_node)

Kim ElQ
Associate II
Posted on September 05, 2017 at 12:15

Hello , 

i'm using murata's module CMWX1ZZabz including stm32l0,  with the provided lorawan_cube code , here is the lowpower_handler fontion, anyone has an idea how to control the MCU wakeup.

in addition to that, the consumption is high in sleep_mode : 1.5mA instead of ~5uA .

Thank you

void LowPower_Handler( void )

{

DBG_GPIO_RST(GPIOB, GPIO_PIN_15);

DBG_GPIO_RST(GPIOB, GPIO_PIN_14);

if ( LowPower_State == 0 )

   {

         HW_EnterStopMode( );

         /* mcu dependent. to be implemented by user*/

         HW_ExitStopMode();

         DBG_GPIO_SET(GPIOB, GPIO_PIN_15);

         HW_RTC_setMcuWakeUpTime( );

   }

else

   {   

         DBG_PRINTF_CRITICAL('z\n\r');

         HW_EnterSleepMode( );

         DBG_GPIO_SET(GPIOB, GPIO_PIN_14);

   }

}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0