STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L162

Posted on January 24, 2018 at 20:29Hi,What is a start point for using STM32L162?

STM32L476 USB_OTG can't get recognized by Windows

Posted on January 25, 2018 at 21:23Version:1.0 StartHTML:0000000168 EndHTML:0000000993 StartFragment:0000000435 EndFragment:0000000976I have configured the USB_OTG as a mass storage on STM32L476VE that has a 8MHz external crystal, and when I connect...

CAN Controller TX does not show signs of life

Posted on January 24, 2018 at 03:15Can_TX is showing no activity. I can't figure out what I am doing wrong. I've set up the project with STMCubeMX to use CAN1 on PD0 and PD1. When I attempt to transmit there is no signs of life on the TX pin. Using ...

tyler2 by Associate II
  • 2166 Views
  • 4 replies
  • 0 kudos

Resolved! EXTI handler gets stuck

Posted on January 24, 2018 at 20:27 With my STM32F4 I am trying to use an external interrupt to read aquadrature encoder on PC02 and regular port PC The interrupt on PC02 fires when I move the encoder, but it won’t return to the main loop again a...

STM32f429 +TFT 1024 x600

Posted on January 25, 2018 at 16:26Hello All I am sorry to disturb you all ; I am trying to fill the lcd structure with the right values but I think I have problem in understanding it please could you help me ? and I see that they are flickers on th...

Resolved! STM32CubeMX for STM32L4 Discovery kit IoT node (B-L475E-IOT01A)

Posted on September 21, 2017 at 03:47Hi,I would like to generate the code by using STM32CubeMX for STM32L4 Discovery kit IoT node (B-L475E-IOT01A).But I don't see the STM32L4 Discovery kit IoT node in the Boards List.Could you suggest for me?Thank y...

Good B by Associate II
  • 2212 Views
  • 6 replies
  • 0 kudos