cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with TimerTick and uwTick

LMI2
Lead
Posted on October 17, 2017 at 00:54

I cant get the STM32F746 timer tick interrupt to work even though I have followed the chain to the tick ISR. Comments in the code are a bit unclear too.

/** @addtogroup HAL_Private_Variables
 * @{
 */
__IO uint32_t uwTick;
/**
 * @brief Provides a tick value in millisecond.
 * @note This function is declared as __weak to be overwritten in case of other 
 * implementations in user file.
 * @retval tick value
 */
__weak uint32_t HAL_GetTick(void)
{
 return uwTick;
}

�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

The uwTick is in private section. But I don't know what it really is. In the code it is said to be a global variable but it isn't because if I use it in my main.c, I get an undeclared error.

By the way, I'm trying to make my own callback work. Similar code has worked before but not now.

(volatile int own, own2=0;)

void HAL_SYSTICK_Callback(void)
{
 own2++;
//uwTick++; //uncommenting this gives an error.
if (own2>1000)
{
own2=0;
own++;
}
}�?�?�?�?�?�?�?�?�?�?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0