STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F746ZG STM32F767ZI unexpected, unwanted Reset

Posted on February 03, 2017 at 17:20I use NUCLEO-F746 and NUCLEO-767, CubeMX 4.19 with FreeRTOS and LWIP.No Watchdog, enough space for sprintf() stack behaviour and SRAM1 only.DC power comes from a DCDC 24/5V converter, super clean, monitored by Osc...

Resolved! [Solved] Linker script: block RAM for variables

Posted on October 04, 2017 at 20:09How do I have to configure the linker script file to block the required spacefor Ethernet buffers at 0x24000000?STM32H743 starts with DTCM at 0x20000000, but Ethernet works in 0x24000000 only.I want to use the RAM ...

Resolved! STM32H743 placing .data or .bss in RAM_D2 = Hard Fault

Posted on January 21, 2018 at 01:31Which step is neccessary to have .data and .bss sections in RAM_D2?If I place them in domain D2, HardFault_Handler() is called. Why?There are known bugs in hal_spi.c - Ethernet works sometimes (if you correct the P...

Xbee STM32F4/7 USRT DMA

Posted on August 30, 2017 at 20:32Hi,When using normal transmit on UART i can send a message from a router to a coordinator without no issueHAL_UART_Transmit(&huart2, (uint8_t*)xFrame, sLen,100);, but when i try to send it using HAL_UART_Transmit_DM...

STM32F4 USB to SD interface

Posted on January 04, 2016 at 22:50Dear CommunityI tried CLIVE1‘ example (/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F4-Discovery%20USB%20Mass%20st...

jogerh by Associate II
  • 1265 Views
  • 5 replies
  • 0 kudos

Resolved! HAL Timer Interrupt Counter Reset

Posted on February 02, 2018 at 20:43I'm trying to configure timer 7 in one-shot mode on the STM32L431 and am having an issue with my timer IRQ triggering as soon as I enable the interrupt. It seems like its preloaded with the period value, however I...

Konami by Senior II
  • 7659 Views
  • 3 replies
  • 2 kudos

reset circuit problem with stm32f4

Posted on July 02, 2017 at 19:29 Hello, I'm using stm32f407vgt6 MCU in a control system and I'm facing a strange problem in the reset circuit, when I power on the system it doesn't start until I put a short circuit wire manually between reset pin a...

Flash content cleared on site?

Posted on February 07, 2018 at 12:33We use STM32F429II on our project.We had over 30 systems running in our lab without problem. Just sent a unit to a remote location, and after few days of continues running, the option register was set to 1 on all ...