cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 HAL UART TX DMA

Lalit B
Associate
Posted on October 19, 2017 at 22:37

Hello,

I'm new to STM32F7 and not familiar with the design environment. I'm setting up 2 UART channels and in CubeMX I setup each UART channel to use normal DMA buffer instead of circular.  Here is a sample of what I'm trying to do.

HAL_UART_Init(&huart1);

HAL_UART_Init(&huart6);

uint8_t buffer1a[] = {0xFF, 0xD7};

uint8_t buffer1b[] = {0xFF, 0xCF, 0x00, 0x00, 0x00, 0x0A, 0x00, 0x32, 0x00, 0x46, 0xF8, 0x00};

HAL_UART_Transmit_DMA(&huart1, buffer1a, sizeof(buffer1a));

HAL_UART_Transmit_DMA(&huart6, buffer1a, sizeof(buffer1a));

HAL_Delay(500);

while (1)

{

HAL_UART_Transmit_DMA(&huart1, buffer1b, sizeof(buffer1b));

HAL_UART_Transmit_DMA(&huart6, buffer1b, sizeof(buffer1b));

HAL_Delay(1000);

}

I need to change buffer1b in the while(1) loop and send out new data.

The first 2 DMA transfers work fine but the DMA transfers in the while(1) loop does not work at all.

What do I need to get this working.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0