User Activity

Posted on November 06, 2017 at 23:55I'm setting up a UART channels to transmit and receive from a slave device.I have Transmit working as I can see the slave is doing what's asked from the command sent to it.On each command the slave reply's back wi...
Posted on October 19, 2017 at 22:37Hello,I'm new to STM32F7 and not familiar with the design environment. I'm setting up 2 UART channels and in CubeMX I setup each UART channel to use normal DMA buffer instead of circular.  Here is a sample of what ...