STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Typo in STM32L1 HAL for EEPROM Erase

Posted on February 12, 2018 at 10:44 Hi, it seems in theSTM32Cube_FW_L1_V1.8.1 in Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash_ex.c there is a typo in the parameter guarding. in line 811: HAL_StatusTypeDef HAL_FLASHEx_DATAEEPROM_...

S H by Associate
  • 773 Views
  • 0 replies
  • 0 kudos

The code is not generated properly.

Posted on February 12, 2018 at 01:08Hello,I have an issue when generate code using STM32CubeMX.At first, it worked properly.The generated code was fine.But I changed the Project Settings from HAL driver to LL driver then the code is not generated pr...

0690X00000609gjQAA.png
dspark by Associate II
  • 1647 Views
  • 2 replies
  • 0 kudos

CubeMX STM32L433CC ETR2 Input bug?

Posted on March 06, 2017 at 17:48 Hi When TIM2 of this device is configured according to the screenshot, the following code will be generated: void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle) { GPIO_InitTypeDef GPIO_InitStruct;...

Losing color depth

Posted on February 12, 2018 at 01:45I've been working on a simple UI library for my project.I'm using the stm32F7 with LTDC configured to RGB888 color space.Whilst I was writing a color gradient function, I noticed that my gradients looked 'choppy'L...

0690X00000604NDQAY.jpg

F767 micro SD card freezes

Posted on February 12, 2018 at 09:40I'm experiencing random freezing of the micro SD card on a custom board, running the STM32F767II.During read operations, occasionally communications is lost to the card and the driver code will experience repeatin...

STM32L151 touch sesing

Posted on February 12, 2018 at 07:03Hi all,I want to enable touch sensing in L151. I used Cube to configure and when I go to configuration tab and click on TS, I get a pop-up showing 'Cube does not support configuration of this IP mode. You can conf...