STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBD_CDC_Init BUG ?

Posted on March 16, 2018 at 15:41Hi, i generated a little project with STMCUBE (Version 4.25.0 and packages 1.21.0)  for STM32F415 with FreeRTOS  and only CDC inteface, but not work.During the INIT on comand 'Set configuration = 1' i receive a error...

Marco1 by Associate II
  • 756 Views
  • 0 replies
  • 0 kudos

Duplicated code in stm32l0xx_hal_pcd.c V1.8.0

Posted on January 22, 2017 at 00:58Hello,I just started a mini project using USB CDC with STM32CubeMX and while trying to figure out how to use CDC driver i found this piece of code.I think there is code duplication (copy-paste) in STM32Cube_FW_L0_V...

STM32F103C8t - CAN problem

Posted on March 15, 2018 at 22:24Hello guys!I am new in using CAN interface, and for the first time, I started to use it in my project. I used STM32F103C8t. When I wanted to use CAN interface, there only happens time-out exception in run-time and I ...

abbas by Associate II
  • 2895 Views
  • 5 replies
  • 0 kudos

Temperature Problem with STM32F429 BGA Board

Posted on March 15, 2018 at 16:06Hello,we have some temperature problems with STM32F429 (BGA) controller boards. If the temp. exceeds by some boards 40°C, and other boards at 60°C the internal voltage regulator shut down, measured at VCap1 & 2. Ev...

Marc T by Associate II
  • 2873 Views
  • 5 replies
  • 0 kudos

Resolved! STM32Cubemx stuck in ''Generating user source code''

Posted on April 08, 2017 at 08:29Hello, I recently installed cubemx 4.20 latest version 4.20.1I can generate the project only 1 time, later if i try to update the project by adding new peripherals, i can not able to generate the code, the whole appl...

n.serina by Associate III
  • 16607 Views
  • 29 replies
  • 0 kudos

STM32L071KBUx UFQFPN32 exposed pad

Posted on March 15, 2018 at 12:13I'm drawing a new design with the STM32L071KBUx #UFQFPN32. Do I have to connect the exposed pad to the GND, or can I leave it open. I don't see any note in the datasheet DM00141136.pdf, so I think that I can leave it...

How to stack IHM03A demo boards?

Posted on March 16, 2018 at 08:53The 'Quick start guide' for STEP01 demo boards says you can stack up to three boards and explains how to set the link resistors to daisy-chain the SPI comms. Fine, but that still leaves all the boards connected to th...

estie by Associate II
  • 751 Views
  • 0 replies
  • 0 kudos