Skip to main content
chris puglia
Visitor II
November 17, 2017
Question

External SRAM with STM32L496

  • November 17, 2017
  • 1 reply
  • 795 views
Posted on November 17, 2017 at 23:06

Hello,

I am trying to find examples of code where the external SRAM is mapped using the linker file. I saw an example of it being done here (

https://community.st.com/0D50X00009XkfB3SAJ

 ). However, all the uses of the SRAM eg.[the  HAL_SRAM_Write_32b() function] in the example code make use of locking. If anyone has examples of using external RAM as general purpose RAM it would be greatly appreciated. 

FYI this is being done on the STM32L496G-DISCO board

null
    This topic has been closed for replies.

    1 reply

    Madhan Mohan Gundluru
    Visitor II
    November 24, 2017
    Posted on November 24, 2017 at 15:24

    Hello Chris, did you able to success with external SRAM access?