cancel
Showing results for 
Search instead for 
Did you mean: 

storing GPS data in a buffer via USART1 on STM32L072CZ

SARTHAK KELAPURE
Associate II
Posted on November 23, 2017 at 12:01

Hello everyone, I am using STM32L072CZ board to get data from GPS on USART1 but when I try to store it onto a buffer, I am losing data bytes. I am putting a small code snippet here, not the final version but somewhere what I am trying to do

for(int i=0;i<500;i++)

{

buffer[i]=USART1->RDR;

}

for(int i=0;i<500;i++)

{

LPUART1->TDR=buffer[i];

}

I am losing most of my data during this process. Please help.

#stm32l0-stm32l0-discovery #gps #usart1-commun #serial-port #communication
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on November 23, 2017 at 13:31

You can't just jam data into the registers. You need to wait on TXE or RXNE bits to assert in SR or ISR register. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3
Posted on November 23, 2017 at 13:31

You can't just jam data into the registers. You need to wait on TXE or RXNE bits to assert in SR or ISR register. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AvaTar
Lead
Posted on November 23, 2017 at 13:53

And GPS (I assume NMEA0183) has strings of variable length, with defined start and end characters.

Not gonna be that simple.

Andrew Neil
Super User
Posted on November 23, 2017 at 17:16

for(int i=0; i<500; i++)
{
 buffer[i] = USART1->RDR;
}�?�?�?�?

Think:

  1. how long will it take to execute 1 iteration of that loop?
  2. how long does 1 character take to complete at whatever baud rate you're using?
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.